LTE FDD

Full-filled Config (Downlink E-UTRA)

For Waveform Playback (ARB) capability.

The Full-filled Config button is displayed when a Downlink E-UTRA carrier is added. Clicking this button opens the Full-filled Preset Config dialog that allows you to set the channels with fully filled DL-SCH configuration. 

SCPI Command 

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<n>:DLINk:CONFig:FFILled <string>

SCPI Example 

RADio:LTEFdd:WAVeform:CCARrier:DLINk:CONFig:FFILled "SystemBandwidth:B10M,Modulation:QPSK" 

Notes

Sets only (Immediate Action)  
<string>: "name:value,name:value,..." 

Preset 

Refer to the element definition of the data part below. 

State Saved 

No 

Range 

Refer to the element definition of the data part below. 

Initial S/W Revision 

A.20.01

Element definition of the data part

The preset value is same as the default value of each setting definition. 

Settings 

Symbols in the data part 

Values in the data part 

Preset values 

System Bandwidth 

System Bandwidth 

B1M4 | B3M | B5M | B10M | B15M | B20M 

B10M 

Modulation 

Modulation 

 QPSK | QAM16 | QAM64 | QAM256 

QPSK